i.mx RT1050: Boot from SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx RT1050: Boot from SPI

1,410 Views
christiangradl
Contributor III

Hi,
can i.mx RT1050 boot from a SPI Flash (e.g. Winbond W25N01GVZEIG)? Is this possible with FlexSPI?

Labels (1)
4 Replies

953 Views
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 Kudos

953 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Could You provide more detailed description of the nxp-sec-boot-ui in English

(only introduction is available now)?

Regards,

Yuri.

0 Kudos

953 Views
jay_heng
NXP Employee
NXP Employee

Hi Yuri,

  English version user guide is available now.

Best Regards,

Jay

953 Views
art
NXP Employee
NXP Employee

Q. Can i.mx RT1050 boot from a SPI Flash (e.g. Winbond W25N01GVZEIG)?

A. Yes, it can.

Q. Is this possible with FlexSPI?

A. Yes, it is possible.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos