i.MXRT1064 EVK SD Card speed issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1064 EVK SD Card speed issue

1,085 Views
robertsonics
Contributor I

I'm using a GPIO pin and scope to time how long it takes to read a block of 4 sequential sectors from the microSD card on the MXRT1064 eval board. I'm used to seeing something on the order of 500 us or less on other processors, but am seeing more like 2 ms with this board. After stepping through the code, it's seems clear that a call to USDHC_SetAdmaTableConfig() is returning an error causing DMA to be disabled and the code to fall back to using polling mode.

The microSD card I'm using reports it's using timing mode SDR104, Freq : 198MHz

Any thoughts as to why the DMA is not being used? This happens with the unmodified "sdcard_interrupt" example project.

Labels (1)
0 Kudos
Reply
1 Reply

986 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, sorry for the later reply.

I debug the <sdcard_interrupt> demo with RT1064_EVK, which is using kUSDHC_DmaModeAdma2 mode.

When debug into USDHC_TransferNonBlocking() function at <fsl_usdhc.c> file, the USDHC_SetAdmaTableConfig() function report success status.

I am testing with SDK V2.6.0 software package for RT1064.

pastedImage_1.png

Thanks for the attention.

best regards,

Mike

0 Kudos
Reply