Hi NXP.
I write to hear if any camera example code for the i.MX rt1050 is available?
Hi Ming,
Here is the information for the company making the camera module:
Hope this will be useful for you.
Best regards!
/Carlos
Hi Carlos,
thanks for the info. I would like to know the specific part no. I can purchase for mt9m114 and mt7725 which you recommended. Are 16 pin connectors to link the camera sensor to the i.mx rt1050 board included in my purchase?
Hi Ming,
i.MXRT1050 EVK designed with both MT9M114(720P) and MT7725(VGA).
And next SDK release will have MT9M114 support by default.
Hope this will be useful for you.
Best regards!
/Carlos
Hi,
In order to have the camera example working, you need to ensure your board version, considering the following note from “MIMXRT1050 EVK Extension Feature Enablement Guide” document:
Hope this will be useful for you.
Best regards!
/Carlos
Oh nice. The camera example was just made available in a user guide.
Hi Thomas,
Yes, a camera example is included as “CSI” of the “i.MXRT1050 EVK Extended Feature Example Code and HW guide”, available at the link below:
In case of requiring other examples, you could get the SDK for i.MX RT. For further details, take a look at the following thread:
https://community.nxp.com/thread/464274
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kyle,
At this time, just the mentioned examples are available, the "Extended Feature Example Code" package without MCUXpresso support, and the "SDK for i.MX RT", including MCUXpresso support.
Hope this will be useful for you.
Best regards!
/Carlos
Hi Carlos,
I have been concerned about this for a long time.
Will the official add the CSI example code for running on MCUXpresso IDE?
If yes, when is the schedule?
Thanks a lot.
Sincerely,
Stuart