i.MX rt1050 camera example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX rt1050 camera example

9,964 次查看
thomasnielsen
Contributor II

Hi NXP.

I write to hear if any camera example code for the i.MX rt1050 is available?

标签 (1)
标记 (2)
12 回复数

7,863 次查看
mingyang
Contributor I

Hi please let me the possible camera modules to use and if possible attach the link for me to purchase it too. In a rush, for an ongoing project that needs it. thank you.

0 项奖励
回复

7,863 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Ming,

Here is the information for the company making the camera module:

http://gb.htkjks.com/

Hope this will be useful for you.

Best regards!

/Carlos

0 项奖励
回复

7,863 次查看
mingyang
Contributor I

current sdk supports mt7725?

0 项奖励
回复

7,863 次查看
mingyang
Contributor I

Hi Carlos,

thanks for the info. I would like to know the specific part no. I can purchase for mt9m114 and mt7725 which you recommended. Are 16 pin connectors to link the camera sensor to the i.mx rt1050 board included in my purchase?

0 项奖励
回复

7,864 次查看
mingyang
Contributor I

Hi, may i know what camera you are using for the i.mxrt1050.

What other cameras are compatible with the i.mx rt1050?

0 项奖励
回复

7,864 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Ming,

i.MXRT1050 EVK designed with both MT9M114(720P) and MT7725(VGA).

And next SDK release will have MT9M114 support by default.

Hope this will be useful for you.

Best regards!

/Carlos

0 项奖励
回复

7,864 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

In order to have the camera example working, you need to ensure your board version, considering the following note from “MIMXRT1050 EVK Extension Feature Enablement Guide” document:

note csi.png

Hope this will be useful for you.

Best regards!

/Carlos

0 项奖励
回复

7,864 次查看
thomasnielsen
Contributor II

Oh nice. The camera example was just made available in a user guide.

Thanks NXP :smileyhappy:
0 项奖励
回复

7,864 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Thomas,

Yes, a camera example is included as “CSI” of the “i.MXRT1050 EVK Extended Feature Example Code and HW guide”, available at the link below:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

In case of requiring other examples, you could get the SDK for i.MX RT. For further details, take a look at the following thread:

https://community.nxp.com/thread/464274

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,864 次查看
kyleyang
Contributor IV

Hi Carlos,

Thanks, but this Feature Example Code did not support MCUXpresso.

Is there any other document about porting the example code?

Thanks.

0 项奖励
回复

7,864 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kyle,

At this time, just the mentioned examples are available, the "Extended Feature Example Code" package without MCUXpresso support, and the "SDK for i.MX RT", including MCUXpresso support.

Hope this will be useful for you.

Best regards!

/Carlos

0 项奖励
回复

7,864 次查看
stuartchen
Contributor I

Hi Carlos,

I have been concerned about this for a long time.

Will the official add the CSI example code for running on MCUXpresso IDE?

If yes, when is the schedule?

Thanks a lot.

Sincerely,

Stuart

0 项奖励
回复