i.MX RT685 Audio Codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT685 Audio Codec

3,274件の閲覧回数
mark_wu
Contributor II

Hello,

i.MX RT685 have a Audio DSP, but in MIMXRT685-EVK use WM8904 for audio codec,

so why not use RT685 DSP processor as  audio codec?

Does the chip support codec? Audio can be output directly

Thanks.

pastedImage_1.png

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,030件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Mark,

 

The Cadence Xtensa HiFi 4 Audio DSP engine is a highly optimized audio processor designed especially for efficient execution of audio and voice codecs and pre- and post-processing modules.

 

What we are implementing in our audio DSP software is the following:

 

The WM8904 codec receives the audio signal from the player such as MP3 or PC. HiFi continuously receives the PCM signal of codec through one I2S interface, and uses another I2S interface to send PCM signal to codec and playback in real time. Please check the below snippet.

pastedImage_2.png

For additional information I recommend you to check the following application notes.

https://www.nxp.com/docs/en/application-note/AN12749.pdf

https://www.nxp.com/docs/en/application-note/AN12762.pdf

I hope this helps.


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,030件の閲覧回数
colinr
Contributor II

Hi Felipe,
I find the application note software downloads on the iMX RT600 product webpage, but can't seem to find these — am I looking in the wrong place?
Regards,
Colin

0 件の賞賛
返信