i.MX RT1176 program to SD/EMMC and debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1176 program to SD/EMMC and debugging

ソリューションへジャンプ
1,533件の閲覧回数
JayCao
Contributor III

Hello all,

I am working on a project using SD/EMMC to store Firmware instead of Flash memory.

I have some questions as below:


1. Is there any guide to do that on RT1176?

I followed the guide below but did not work on our EVKs.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1050-SDRAM-app-code-boot-from-SDcard-burn-with...


2. Do we need to load any bootloader first and then follow the guide in 1st question for it to work?

3. How to debugger the firmware ?

Hope to hear from you soon.

Best regard,

Tu

タグ(4)
0 件の賞賛
返信
1 解決策
1,464件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1 返信
1,465件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Please refer to our previous post for the solution: https://community.nxp.com/t5/i-MX-RT/LED-cannot-blinking-when-loading-firmware-via-SDcard/td-p/18345...

Wish you have a nice day!

0 件の賞賛
返信