i.MX RT1170 CAN bootloder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT1170 CAN bootloder

1,903 次查看
scarletlee
Contributor III

Hi,

Have a CAN bootloader for i.MX RT1170?

I tried to search bootloader information but only USB bootloader.

Thanks.

标记 (1)
0 项奖励
回复
3 回复数

1,893 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Have a CAN bootloader for i.MX RT1170?
-- The Serial Boot doesn't support other peripherals except for the UART and USB, so it needs the developers to implement a secondary bootloader that supports the CAN interface.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,879 次查看
scarletlee
Contributor III

Hi Jeremy,

 

Thanks for your reply.

So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?

 

Best Regards,

Scarlet

0 项奖励
回复

1,874 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1)So...your mean is CANBUS bootloader must developer by myself or maybe NXP can provide an example?
-- As I know, there's no similar demo now for you to refer to.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复