i.MX RT1064 external CLK1 input usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT1064 external CLK1 input usage

跳至解决方案
2,521 次查看
_Chris_
Contributor II

Hi,

At this moment I'm evaluating the i.MX RT1064 with the MIMXRT1064-EVK which is going well.
For future product development we are investigating the possibilities for this processor to clock some external peripherals with a clock derived from a source other than the 24MHz.

For this the i.MX RT1064 seems to provide an external CCM_CLK1_P/CCM_CLK_N input which can be selected by using the MCUXpresso IDE clock configurator.

However the design documentation is not clear about this function, the "i.MX RT Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor (REV 4)" states in Table 4. on page 9:

_Chris__0-1614158294779.png

While in the "i.MX RT1064 Crossover Processors Data Sheet for Consumer Products, Rev. 2, 08/2020" states in chapter 3.1 on page 16:

_Chris__1-1614158702239.png

The question is, which of the table is correct, can this input be used for normal operation or not ? and if so has this any side effects which should be taken into account ?

Best Regards,

Chris

 

标签 (1)
0 项奖励
回复
1 解答
2,491 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Chris,

They are "manufacturing of the chip / internal use by NXP".

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,510 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Chris,

I think you'd better leave these pins unconnected. In fact, in hardware development guide Rev.2 this two pins can be used to input clock. So, I think this is not a typo.

 

Regards,

Jing

0 项奖励
回复
2,506 次查看
_Chris_
Contributor II

Hi Jing,

I'm afraid my question wasn't clear, so let's rephrase my question.

The problem I have is I would like to use these pins as an external clock source as mentioned in the "i.MX RT1064 Crossover Processors Data Sheet for Consumer Products, Rev. 2, 08/2020".

However the "i.MX RT Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor (REV 4)" states "it is for internal use only" "It is used only for internal test, please make CLK1_N/P pairs remain unconnected."

Which suggests I can't use them because they are for "internal use ony".

Are these pins supposed to be used for clocking in normal use,  or is it only used during "manufacturing of the chip / internal use by NXP" ?

Best Regards,

Chris

 

0 项奖励
回复
2,492 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Chris,

They are "manufacturing of the chip / internal use by NXP".

 

Regards,

Jing

0 项奖励
回复