Hi,
I try to use the SEMC in DBI mode in order to interface an TFT-LCD with 8bits 8080 type interface. Here is my SMEC initialization code:
/* Init SEMC perfieral */
semc_config_t semc_config;
SEMC_GetDefaultConfig(&semc_config);
semc_config.dqsMode = kSEMC_Loopbackinternal; /* For more accurate timing. */
SEMC_Init(SEMC, &semc_config);
/* Configure the SEMC module to inteface to the display, "DBI" mode */
status_t config_res;
semc_dbi_config_t dbi_config;
dbi_config.csxPinMux = kSEMC_MUXA8;
dbi_config.address = 0x80000000;
dbi_config.memsize_kbytes = 128;
dbi_config.columnAddrBitNum = kSEMC_Dbi_Colum_12bit;
dbi_config.burstLen = kSEMC_Dbi_BurstLen1;
dbi_config.portSize = kSEMC_PortSize8Bit;
dbi_config.tCsxSetup_Ns = 100;//50;
dbi_config.tCsxHold_Ns = 100;//50;
dbi_config.tWexLow_Ns = 100;//40;
dbi_config.tWexHigh_Ns = 100;//40;
dbi_config.tRdxLow_Ns = 100;//90;
dbi_config.tRdxHigh_Ns = 100;//70;
dbi_config.tCsxInterval_Ns = 100;//50;
config_res = SEMC_ConfigureDBI(SEMC, &dbi_config, CLOCK_GetFreq(kCLOCK_SemcClk));
if(config_res != kStatus_Success)
{
printf("Error: Failed to initialize SEMC DBI!\n");
}
Note that on this code, I've increased the timing temporary to improve debugging with logic analyser.
To write the data to the Display I then write to the address 0x80000000 for command and 0x80010000 for data by de-referencing a pointer on an unsigned char. This all seems to work, but when I try to send on byte, it appears that the SEMC sends out 8 bytes! See the logic analyser capture bellow where 0x30 is supposed to be sent:
Any Idea what could code those 8 bytes to be sent instead of 1 byte ?
Also, can you please help me to understand the "columnAddreBitNum" and "busrtLen" ? Those totally make sens for other type of memory (SDRAM, Flash...) but not for a display. I don't know why we have to give a memory size, as TFT with controller is only two address cells (one for commands, one for data, the address bit controlling the D/CX signal).
If some one has a code example using SEMC in DBI mode that would be greatly appreciated (there is none in the SDK).
Thanks!
Antoine
Solved! Go to Solution.
Yes, data and command are inverted in my description, but this is not the cause of having 8 bytes send out. After reading lot of doc, I discovered the cause of this: The SEMC module is attached to the AXI bus wich is 64bit, hence the 8 bytes out even if the software use 1 byte.
The solution is to use the IP bus instead of dereferencing the 0x80000000 address space. There is a function in the SDK for that:
SEMC_SendIPCommand(SEMC, kSEMC_MemType_8080, (uint32_t)d0x80000000, kSEMC_NORDBICM_Write, cmd_byte, NULL);
Note that I tried the init code from https://community.nxp.com/thread/497507 but with no different result.
Hi,
First of all, sorry for the later reply.
From below Note, I think your DBI operation is incorrect:
From your descripton:
To write the data to the Display I then write to the address 0x80000000 for command and 0x80010000 for data by de-referencing a pointer on an unsigned char.
You do the incorrect opreation, you shoulld write to the address 0x80010000 for command and 0x80000000 for data by de-referencing a pointer on an unsigned char.
Wish it helps.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes, data and command are inverted in my description, but this is not the cause of having 8 bytes send out. After reading lot of doc, I discovered the cause of this: The SEMC module is attached to the AXI bus wich is 64bit, hence the 8 bytes out even if the software use 1 byte.
The solution is to use the IP bus instead of dereferencing the 0x80000000 address space. There is a function in the SDK for that:
SEMC_SendIPCommand(SEMC, kSEMC_MemType_8080, (uint32_t)d0x80000000, kSEMC_NORDBICM_Write, cmd_byte, NULL);