i.MX RT1060 Serial Internal Boot Mode with LPUART1 Connected to USB-Serial Cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1060 Serial Internal Boot Mode with LPUART1 Connected to USB-Serial Cable

Jump to solution
642 Views
MulattoKid
Contributor IV

Hi,

I'm experiencing a strange issue on a RT1060 where if I have the boot pins configured as internal boot and have a USB-Serial cable connected to LPUART1 (which is used when in Serial Downloader mode) the MCU seems to crash. It doesn't boot the FW and doesn't enter Serial Downloader mode (Secure Provisioning Tool is unable to connect).

I've narrowed it down to the LPUART1_RXD (GPIO_AD_B0_13) being connected. Without it being connected the MCU boots fine. It also seems to persist between resets. I.e. if I power on the MCU with LPUART1_RXD connected to the USB-Serial cable it doesn't boot, and if I disconnect LPUART1_RXD and reset the MCU it still doesn't work, but if I power cycle after disconnecting LPUART1_RXD it works.

Any ideas what could cause this? Does the boot ROM read the state of LPUART1_RXD even in internal boot mode (but a reset should re-trigger any logic related to that, right)?

Thanks,
Daniel

Labels (1)
0 Kudos
Reply
1 Solution
621 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, hope you are well.

It is not suggested having signal applied to the pins before powering up the MCU, this may lead to issues like booting.
First, the ROM code polls the UART1 signals from TXD1/RXD1. Add a 10-kΩ pull up resistor to the TXD1/RXD1 pins to avoid an invalid trigger of the UART port.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
2 Replies
622 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, hope you are well.

It is not suggested having signal applied to the pins before powering up the MCU, this may lead to issues like booting.
First, the ROM code polls the UART1 signals from TXD1/RXD1. Add a 10-kΩ pull up resistor to the TXD1/RXD1 pins to avoid an invalid trigger of the UART port.

Best regards,
Omar

0 Kudos
Reply
526 Views
MulattoKid
Contributor IV

Hi @Omar_Anguiano,

Thank you for the information!

0 Kudos
Reply