i.MX RT1050 SJC Secure Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1050 SJC Secure Mode

1,203 Views
bdc
Contributor I

hello,

I am trying to use the Secure Mode in the i.MXRT 1050 Secure JTAG Controller. The SRM documentation describes the activation of the JTAG in secure mode in section  11.5.1.2.1.

Of course, this requires setting in fuse map SJC_RESP desired value at 0x600 (7 bytes), and JTAG_SMODE at 0x460[23:22] to 01.

My question is, what is the tool/procedure to interact with the TAP controller to send the proper instructions and to get challenge code, present response, and validate that the authentication is successful ? I have a Segger J-Link probe, and I am using MCUXpresso IDE. with a IMXRT1050-EVKB.

Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,020 Views
michael_galda
NXP Employee
NXP Employee

Hi Benjamin,

Here is Michael,

I found this thread on NXP community.

Sorry for bothering.

Q: Have you ever make the Secure JTAG Challenge-Response authentication working with Segger J-Link or anything else?

Thanks and regards,

Michael

0 Kudos
Reply

1,020 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The following may be helpful:

IDE with support Secure JTAG 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply