i.MX RT power-up/power-down sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT power-up/power-down sequence

1,673 Views
gfisys
Contributor I

Hi, I have a couple of questions regarding power-up/power-down sequencing and the use of external DCDC converter.

1. The recommended power control scheme is this:

2020-12-10 17_50_44-MIMXRT1010HDUG - Hardware Development Guide for the MIMXRT1020.pdf - Adobe Acrob.png

I can clearly see that this scheme satisfies the power-up sequence requirement which says SNVS_IN must be powered prior to all other modules. However, I failed to see how this will satisfy the power-down sequence requirement that says SNVS_IN supply must be turned off after any other supplies. When the 5V source supply is turned off everything will power down at virtually the same time, no?

 

2.  I have seen some custom board designs, including some commercial ones) featuring i.MX RT chips that do not use any external DC/DC component, which means the power-up/power-down sequences are not being implemented, and yet these designs work, haven't seen them failed yet. Can NXP/anyone shed some light as to why these designs work? To see this is done for a commercial product seems to suggest that the designers must have a high level of confidence about this.

 

Regards,

Henry

0 Kudos
Reply
1 Reply

1,654 Views
gfisys
Contributor I

Ok, found the answer in this thread:

https://community.nxp.com/t5/i-MX-RT/IMXRT1064-Power-Up-sequence/m-p/994938

Though it continues to baffle me why the documentation went as far as stating the possibility of "irreversible damage to the processor" when in the end it's so casually mentioned that the external DC/DC circuitry is not absolutely needed.

 

 

0 Kudos
Reply