i.MX RT internal LDO and DC/DC converter's specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT internal LDO and DC/DC converter's specification

1,002 Views
masahirokiniwa
Contributor IV

I checked the data sheet and reference manual for i.MX RT 1050, but I couldn't find some specifications.

Could you tell me below specifications?

<DC/DC converter>

 - Switching frequency

 - Radiation noise on the reference circuit (i.MX RT1050 EVK)

<LDO>

 - PSRR : Power Supply Rejection Ratio

If I can find them by other documents, could you tell me them?

Best regards,

M.Kiniwa

Tags (1)
0 Kudos
Reply
1 Reply

912 Views
art
NXP Employee
NXP Employee

Q. Switching frequency

A. The typical switching frequency of the i.MX RT1050 DCDC converter is 1.6MHz.

Q. Radiation noise on the reference circuit (i.MX RT1050 EVK)

A. Not specified.

Q. PSRR : Power Supply Rejection Ratio

A. Not specified. The only parameter specified here is the LDO output accuracy that is +/- 25mV.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply