i.MX RT 1010 Zephyr OS supported or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 1010 Zephyr OS supported or not?

4,246 Views
andreyloginov
Contributor II

Hi

I am considering to do prototype development using i.MX RT1010 EVK with Zephyr OS but as I see there is some discrepancy in documentation. On NXP docs I see that it is supported by Zephyr OS but I don't see it in the list of supported boards on zephyr wiki. Do I need to port board packages to i.MXRT1010 or will it be supported officially ?
Please advise.

Labels (1)
6 Replies

3,907 Views
SanyaadeAdekoya
Contributor I

I was able to build MicroPython based Zephyr OS for iMX RT on Linux but I have not be able to flash test it due to JTAG winding up.

I might give another try this weekend

God blesses!!!

Best regards,
Sanyaade

0 Kudos
Reply

3,907 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Andrii:

As far as I know, the most up-to-date list is at

Supported Boards — Zephyr Project Documentation 

This page gets regenerated rightly based on the latest source

From that I can see that the following RT boards are supported

pastedImage_2.png

Regards

Daniel

3,907 Views
maureen
NXP Employee
NXP Employee

Hi Andrii,

Yes, RT1010 will be supported. There is a pull request available that we hope to get merged after the Zephyr 2.1 release. Currently the master branch is closed to new features to prepare the release, and will reopen after the release is complete. In the meantime, you can use the pull request branch.

Enable imxrt1010 by jhqian · Pull Request #19335 · zephyrproject-rtos/zephyr · GitHub 

Maureen

3,907 Views
marcomerlin
NXP Employee
NXP Employee

Hi Maureen,

similarly the product page mentions mbed support: will that be provided in the future as well ?

Regards,

MM

0 Kudos
Reply

3,907 Views
maureen
NXP Employee
NXP Employee

Yes

3,907 Views
andreyloginov
Contributor II

Hi

Question is will i.MX RT1010 be supported if yes then when ?

--

Regards,

Andrey Loginov | Solution Architect | ARMA Instruments AG | https://armainstruments.com<https://armainstruments.com/>;

T: +41449746005

0 Kudos
Reply