how do i know if a clock is enabled already?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how do i know if a clock is enabled already?

Jump to solution
1,298 Views
5angxr
Contributor III

If I need to init ADC and QDC,  and they both use XBARA, and `CLOCK_EnableClock(kCLOCK_Xbar1);` is invoked twice.

Would it be a problem that kCLOCK_Xbar1 enable twice? Is there a function I can use to know if the module already has been enabled before I try to enable the module?

0 Kudos
Reply
1 Solution
1,228 Views
Habib_MS
NXP Employee
NXP Employee

Hello @5angxr,

It is not a problem to use "CLOCK_EnableClock(kCLOCK_Xbar1);" twice, this because the clock will be enabled.

Also, to know if the clock is enabled you can see the bits 22 and 23 in the register called "CCM Clock Gating Register 2" where is in the chapter 14.7.23 in the RM. As shows the next image:

Habib_MS_0-1723070379468.png

 

Also, if you experience any issue, do not hesitate to let me know.

BR

Habib

View solution in original post

0 Kudos
Reply
3 Replies
1,254 Views
Habib_MS
NXP Employee
NXP Employee

 

Hello @5angxr,

Sorry for taking a while to get back to you. In order to support you better, can you provide me which RTxxxx you are currently using?

BR

Habib

0 Kudos
Reply
1,244 Views
5angxr
Contributor III
RT1042
0 Kudos
Reply
1,229 Views
Habib_MS
NXP Employee
NXP Employee

Hello @5angxr,

It is not a problem to use "CLOCK_EnableClock(kCLOCK_Xbar1);" twice, this because the clock will be enabled.

Also, to know if the clock is enabled you can see the bits 22 and 23 in the register called "CCM Clock Gating Register 2" where is in the chapter 14.7.23 in the RM. As shows the next image:

Habib_MS_0-1723070379468.png

 

Also, if you experience any issue, do not hesitate to let me know.

BR

Habib

0 Kudos
Reply