Hi
Have a go with this reference:
https://www.utasker.com/iMX/RT1020.html
It shows the board using its QSPI flash as parameter, file system and firmware upload storage.
In order to test your sector number 593 you can use the command line menu (on UART, USB or Telnet) as follows:
Input/Output menu
===================
up go to main menu
md Memory Display [address] [<l>|<w>|<b>] [num]
mm Memory Modify [address] [<l>|<w>|<b>] [val]
mf Memory Fill [address] [<l>|<w>|<b>] [val] [num]
sd Storage Display {as md}
sm Storage Modify {as mm}
sf Storage Fill {as mf}
se Storage Erase [address] [len-hex]
sr Status read
sw Status write
set_ddr Set port type [1..4] [<i>|<o>
get_ddr Get data direction [1..4]
read_port Read port input [1..4]
write_port Set port output [1..4] [0/1]
out output value [hex]
save Save port setting as default
help Display menu specific help
quit Leave command mode
#sd 60251000 b 100
Memory Display
0x60251000 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251010 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251020 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251030 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251040 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251050 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251060 ff ff ff ff ....
sm 60251000 b 55
Write - OK
sd 60251000 b 10
Memory Display
0x60251000 55 ff ff ff ff ff ff ff ff ff U.........
#sf 60251001 b 77 17
Fill - OK
sd 60251000 b 30
Memory Display
0x60251000 55 77 77 77 77 77 77 77 77 77 77 77 77 77 77 77 Uwwwwwwwwwwwwwww
0x60251010 77 77 ff ff ff ff ff ff ff ff ff ff ff ff ..............
#se 60251000 1
Erased
sd 60251000 b 30
Memory Display
0x60251000 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
0x60251010 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ..............
I am wondering whether your command should use
flexspi_nor_flash_erase_sector(EXAMPLE_FLEXSPI, (0x60000000 + (593 * SECTOR_SIZE)));
or whether your problem is that you have XIP code running in the spi flash device when you try to erase it, which would also fail.
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]