ecompass_cm7 sample project cannot see FXOS8700 on MIMXRT1170-EVK board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ecompass_cm7 sample project cannot see FXOS8700 on MIMXRT1170-EVK board

Jump to solution
1,717 Views
kchan
Contributor II

The development PC is Windows 10 Enterprise 21H2.

The IDE is MCUXpresso v11.7.0.

The SDK installed in the IDE is SDK_2.13.0_MIMXRT1170-EVK.

I disconnected J6 and J7 on the eval board and connected Segger JLink to J1.

I connected a USB cable from my development PC to J11 on the eval board.

 

I imported the SDK project ecompass_cm7, under the demo_apps category, and configured the debugger to use JLink to flash the board.  I started the debugger, which stopped at the first line of main() in ecompass.c.  I used the IDE terminal to connect to the USB serial port on the eval board.

I then resumed program execute and observed this print statement showing "Sensor device initialize failed!"

I stopped the debugger and repeated the debug process...it showed the same print statement.

I then imported the MQX accel sample project into the IDE and tried that one.  The terminal tab showed print statements:

Checking I2C 1, device 0x1c...no response
Checking I2C 1, device 0x1d...no response
Checking I2C 1, device 0x1e...no response
Checking I2C 1, device 0x1f...no response
Checking I2C 1, device 0x20...no response

No accelerometer found.

 

I am submitting a picture of the eval board showing my usb to serial and jlink connections.

Thank you in advance for your help!

 

0 Kudos
Reply
1 Solution
1,705 Views
Masmiseim
Senior Contributor I

Hello,

 

as you can see in your picture, the Sensor FXOS8700CQ is not soldered on your board.

So, it is no surprise that you cannot communicate with it.

 

Regards

View solution in original post

0 Kudos
Reply
2 Replies
1,706 Views
Masmiseim
Senior Contributor I

Hello,

 

as you can see in your picture, the Sensor FXOS8700CQ is not soldered on your board.

So, it is no surprise that you cannot communicate with it.

 

Regards

0 Kudos
Reply
1,703 Views
kchan
Contributor II

That would explain it.  Thank you!

0 Kudos
Reply