eclipse photon build of u-boot for iMXRT proc project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eclipse photon build of u-boot for iMXRT proc project

1,276 Views
jautry
Contributor IV

Are there any updates on the procedures for building u-boot on the latest Eclipse Photon.  I have a Fedora host and am trying to set up a debug session but the app notes I see out there are for older versions of Eclipse and I am unable to replicate steps in photon.  eg.  they steps require disabling automated makefile generation, but that disables build settings in photon.  Also not sure what project format to use since they added managed projects.  Has anyone gotten through this with the latest Eclipse?

Tags (1)
0 Kudos
Reply
1 Reply

1,269 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Are there any updates on the procedures for building u-boot on the latest Eclipse Photon
-- In my opinion, you'd better contact Eclipse to apply for this update.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply