does MQTT library support 2 brokers?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

does MQTT library support 2 brokers?

跳至解决方案
2,651 次查看
ping1
Contributor V

Dear all

I am using MQTT library under lwip example, I wonder whether it supports two brokers at same time. If so, how to do it?

Regards!

Ping

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,629 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  Sorry for my misleading previously!

    SDK LWIP can support more than one MQTT broker at one time, you just need to define more MQTT broker, attached code is for your reference, and it has been tested, you can refer to it.

uint8_t *serverName[MAXMQTT_NUM] = {EXAMPLE_MQTT_SERVER_HOST, MQTT_SERVER_HOST2}; 
uint32_t serverPort[MAXMQTT_NUM] = {EXAMPLE_MQTT_SERVER_PORT, MQTT_SERVER_PORT2}; 

for(uint32_t i=0; i<MAXMQTT_NUM; i++)
{
mqtt_client[i] = mqtt_client_new(); 
}

 

for(uint32_t i=0; i<MAXMQTT_NUM; i++)
{
if (ipaddr_aton(serverName[i], &mqtt_addr[i]) && IP_IS_V4(&mqtt_addr))
{
/* Already an IP address */
err = ERR_OK;
}
else
{
/* Resolve MQTT broker's host name to an IP address */
PRINTF("Resolving \"%s\"...\r\n", serverName[i]);
err = netconn_gethostbyname(serverName[i], &mqtt_addr[i]);
}
}

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,615 次查看
mjbcswitzerland
Specialist V

Hi

MQTT operates over a TCP socket or a secure TCP socket and so any number of instances should be possible. This has nothing to do with Ethernet or the number of Ethernet controllers available but is restricted only by the resources available (mainly RAM).

Each MQTT client can have its own MQTT broker settings and behave independently of other MQTT clients that are operating on the top of the same TCP/IP stack.

I don't know details of the LWIP MQTT implementation but with the uTasker MQTT client any number can be used, whereby it is to note that the TLS layer, when using secure MQTT connections is where the most RAM is required and so is more of the practical limit if multiple secure sessions are used in parallel.

Regards

Mark

 

0 项奖励
回复
2,630 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  Sorry for my misleading previously!

    SDK LWIP can support more than one MQTT broker at one time, you just need to define more MQTT broker, attached code is for your reference, and it has been tested, you can refer to it.

uint8_t *serverName[MAXMQTT_NUM] = {EXAMPLE_MQTT_SERVER_HOST, MQTT_SERVER_HOST2}; 
uint32_t serverPort[MAXMQTT_NUM] = {EXAMPLE_MQTT_SERVER_PORT, MQTT_SERVER_PORT2}; 

for(uint32_t i=0; i<MAXMQTT_NUM; i++)
{
mqtt_client[i] = mqtt_client_new(); 
}

 

for(uint32_t i=0; i<MAXMQTT_NUM; i++)
{
if (ipaddr_aton(serverName[i], &mqtt_addr[i]) && IP_IS_V4(&mqtt_addr))
{
/* Already an IP address */
err = ERR_OK;
}
else
{
/* Resolve MQTT broker's host name to an IP address */
PRINTF("Resolving \"%s\"...\r\n", serverName[i]);
err = netconn_gethostbyname(serverName[i], &mqtt_addr[i]);
}
}

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

0 项奖励
回复