camera module on i.MX RT1170 EVK example?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

camera module on i.MX RT1170 EVK example?

Jump to solution
2,668 Views
skruglewicz
Contributor III

Hello

I'm evaluating the  i.MX RT1170 EVK supplied with the kit.

Does anyone know of an SDK example, webinar or blog so I can experiment with it.

Thank in Advance

Steve K

Tags (1)
0 Kudos
Reply
1 Solution
2,659 Views
carstengroen
Senior Contributor II

Steve,

get the SDK for the 1170EVK, there are samples that uses the camera, for example: SDK_2.9.2_MIMXRT1170-EVK\boards\evkmimxrt1170\eiq_examples\tensorflow_lite_label_image

View solution in original post

0 Kudos
Reply
2 Replies
2,660 Views
carstengroen
Senior Contributor II

Steve,

get the SDK for the 1170EVK, there are samples that uses the camera, for example: SDK_2.9.2_MIMXRT1170-EVK\boards\evkmimxrt1170\eiq_examples\tensorflow_lite_label_image

0 Kudos
Reply
2,652 Views
skruglewicz
Contributor III

HI carstengroen

Thank you for the reply. I found the example in the SDK and have loaded it into my workspace. I will start experimenting with it soon.

I'm trying to use the camorra module in  code that I'm designing and this will help me to learn how the hardware for the camera is controlled.

At first glance into the code, it looks as if all the interfacing is done in the source\image folder?

Specifically in \source\image\image_capture.c ?

skruglewicz_0-1622907957975.png

 

0 Kudos
Reply