breaks at address "0x20ed4a" with no debug information available, or outside of program code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

breaks at address "0x20ed4a" with no debug information available, or outside of program code

1,026 Views
M_M19
NXP Employee
NXP Employee

Hello, 

I just got my I.MXRT1060 board and was following a tutorial given on this website: Get Started with the MIMXRT1060-EVK | NXP Semiconductors in order to print out my obligatory "Hello World". However, it seems like whenever I click on debug, it breaks at address "0x20ed4a" with no debug information available, or outside of program code (see image below). I am not sure how to fix this issue. 

M_M19_0-1666644740825.png

 

Labels (1)
0 Kudos
Reply
1 Reply

1,015 Views
jay_heng
NXP Employee
NXP Employee

0x20ed4a is in BootROM region, you need to check the board boot mode settings (make sure BOOT_MODE[1:0] is 2'b10)