adjust usdhc bus stength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adjust usdhc bus stength

Jump to solution
798 Views
MCW
Contributor III

Hi all,

 

The strenght of usdhc signal is too strong, so I consider it could reduce the life of imxrt1061.

I find two ways to adjust the strenght of usdhc signal.

1. Change the DSE

The problem of overshoot and undershoot signal is solved when I set to DSE_1_R0_150.

But it causes the other problem whish is the rising time and falling time become longer.

MCW_0-1695350275322.png

2. Use SD_SetDriverStrength()

However, the second way (SD_SetDriverStrength() api) cannot support the sd card without SDR50 mode.

So, is there any other solution to alleviate the strength of usdhc bus signal?

 

Best regards,

Doris

 

 

 

0 Kudos
Reply
1 Solution
740 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MCW ,

SD_SetDriverStrength() change SD card driver strength.

You can refer to table12-2 in RM. It is a matrix of DSE, SPEED and SRE field.

Another way to improve the EMI is add 0 ohm or small resistor into the bus.

 

Regards,

Jing

 

View solution in original post

1 Reply
741 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MCW ,

SD_SetDriverStrength() change SD card driver strength.

You can refer to table12-2 in RM. It is a matrix of DSE, SPEED and SRE field.

Another way to improve the EMI is add 0 ohm or small resistor into the bus.

 

Regards,

Jing