Wire Ack Fault running HelloWorld on RT685-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wire Ack Fault running HelloWorld on RT685-EVK

1,647 Views
tka75
Contributor I

Trying to get an iMXRT685-EVK up running and going through the 'Getting Started with MCUXpresso SDK for RT600' document. I'm not able to run the HelloWorld project and getting the error message shown below. 

Executing flash operation 'Erase' (Erase flash) - Sat Jan 11 12:04:19 CET 2020
Checking MCU info...
Scanning for targets...
Executing flash action...
MCUXpresso IDE RedlinkMulti Driver v11.0 (May 22 2019 13:46:40 - crt_emu_cm_redlink.exe build 6)
( 0) Reading remote configuration
Wc(03). No cache support.
Found chip XML file in C:/nxp/workspace/evkmimxrt685/hello_world/Debug\MIMXRT685S.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
============= SCRIPT: RT600_connect.scp =============
RT600 Connect Script
DpID = 6BA02477
AP not ready
Wire Ack Fault - target connected?
Wire Ack Fault - target connected?
Wire Ack Fault - target connected?
Wire Ack Fault - target connected?
Wire Ack Fault - target connected?
Wire Ack Fault - target connected?
============= END SCRIPT ============================
Probe Firmware: LPC-LINK2 CMSIS-DAP V5.224 (NXP Semiconductors)
Serial Number: KRAWCQCQ
VID:PID: 1FC9:0090
USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#7&a414ab4&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0 after searching for a good core
Failed on connect: Nn(05). Wire ACK Fault in DAP access
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
Debug bus selected: MemAp 0
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.
(100) Target Connection Failed
error closing down debug session - Nn(05). Wire ACK Fault in DAP access
Unable to perform operation!
Command failed with exit code 1

I found some advice (NXP site) on erasing the FLASH but didn't succeed in doing so:

Screen capture attached!FLASH_MassErase.PNG

I'm also working with the iMXRT1060 which hasn't caused similar issues.

Any ideas?

Labels (1)
0 Kudos
Reply
2 Replies

1,472 Views
chaosdefinition
Contributor I

Hi, I'm facing the same problem here.  Could you provide help now?

0 Kudos
Reply

1,490 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Unfortunately, i.MX RT600 has not been officially launched so we cannot provide support.

Sorry for the inconvenience this may cause you.

 

Best regards,

Felipe