Which media processor with low power can be used for Night Vision Thermal imager application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which media processor with low power can be used for Night Vision Thermal imager application

1,246 次查看
subham_p
Contributor I

Dear Sir/ Ma'am

We are looking for Media Processor having ultra low power features and with following interface:

1. 24 bit RGB Camera input with HSYNC,VSYNC,DE

2. 8 bit Parallel Video Input

3. 24 bit Video Output for OLED

4. Analog Video output for 7" LCD

5. SD Card support upto 256GB

6. Keypad Interface

7. Power Consumption should be Less than 1.2W with 1 video input and 1 video output and Keypad running.

标记 (1)
0 项奖励
回复
1 回复

1,132 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Subham

first one can look i.MX comparison table

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

There are no much i.MX processors with several parallel camera inputs, probably

better suitable option would be i.MX6S:

AN4715, i.MX 6Solo Power Consumption Measurement

https://www.nxp.com/docs/en/application-note/AN4715.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复