I'm trying to get to know the wifi_examples/wifi_cli example in the SDK (2_16_100) MIMXRT1170-EVKB. Can anyone tell me what the purpose of the CONFIG_WIFI_SMOKE_TESTS is for? I see that this pulls in the Ethernet interface into the wifi_cli build, but I don't quite follow what the purpose is.
Thanks. I've been looking at the code, but it's just tough to figure out what that macro is for. Right now I'm using the Embedded Artists 2EL M.2 module (WIFI_IW612_BOARD_MURATA_2EL_M2); but that may change.