I purchased the SLN-LOCAL-IOT board, and I have a few questions...
First, I don't yet understand what the i.MX RT106L processor is. I did a search in the forum for RT106L and found very little. I watched the recorded webinar and according to slide 9 of the handout (along with information from the speaker) there is a multi-stage audio-front-end that does a lot of nice stuff; but it is binary-only. That tells me the pipeline is firmware and the source for that firmware is not provided. Is this correct?
As far as I can tell (based on the block diagram on pg 6 of the handout); there's really nothing on the MIMXRT106LDVL6A block that isn't on a RT1062. I haven't found any literature that specifically calls out the RT106L's uniqueness within the i.MX RT106X family. It seems to me that it is a licensing arrangement rather than a unique spin of silicon.
Can someone elaborate on this?
Solved! Go to Solution.
Hello Ed,
Yes, it's spin of the silicon-based on the RT1062 derivative. The RT106L specifically enables software packages that are licensed with this part.
Hi,
RT106L is a Turnkey solution for local voice control, including far-field audio front end and automatics speech recognition engine
which differs from other similar solutions, for example RT106F is a turnkey solution focused on face and emotion recognition
That didn't really answer my question...
Am I correct to assume that "turnkey solution" here means it is a library that comes with an iMXRT1062 or is it a unique spin of silicon? If it is new silicon, where is the datasheet?
Hello Ed,
Yes, it's spin of the silicon-based on the RT1062 derivative. The RT106L specifically enables software packages that are licensed with this part.
Maybe I could help here, RT106L is NXP EdgeReady MCU-Based Solution for Local Voice Control.
according to the factsheet (you can refer https://www.nxp.com/docs/en/fact-sheet/IMXRT106LLVCFS.pdf )
you can see the RT106L MCU part number is MIMXRT106LDVL6A, with the following the link you will be able to find the datasheet:
https://www.nxp.com/part/MIMXRT106LDVL6A#/
Hope that helps you.
Kind regards,
Shai