What is the function of VDD_USB_CAP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the function of VDD_USB_CAP

1,970 次查看
carolyn_zhang
Contributor II

Hi,

It looks like the USB of i.MX RT can be used normally no matter VDD_USB_CAP is floated or not. I just wander what is the function of VDD_USB_CAP. Thanks.

标签 (2)
0 项奖励
回复
3 回复数

1,909 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Carolyn, 

VDD_USB_CAP is the output of the USB_LDO regulator. It's not recommended to leave this pin floating, please refer to the below suggestion: 

pastedImage_1.png

In the case of all our evaluation boards, we use these two capacitors 0.1uF and 10uF. Having these two capacitors help to have a more stable USB voltage. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 项奖励
回复

1,763 次查看
giuseppescarpi
Contributor III

Hi @victorjimenez,

I'd like to follow-up this question.

The board I'm working has very limited room available. I plan NOT to use USB, so the question is: can I leave VDD_USB_CAP floating?

Thanks

Giuseppe

 

0 项奖励
回复

1,909 次查看
carolyn_zhang
Contributor II

Hi, Victor,

Thanks.

0 项奖励
回复