What happens if the transmit ID and receive ID are the same in CAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What happens if the transmit ID and receive ID are the same in CAN?

183 Views
takagi_y
Contributor III

RT1062 When the transmit ID and receive ID are the same value in CAN, the transmitted data is received on the channel it was sent on.


I have a question because there is an error in the settings.


I have confirmed that the LPB of FLEXCANx_CTRL1 is 0.

 

Best regards

Labels (1)
0 Kudos
Reply
1 Reply

148 Views
Habib_MS
NXP Employee
NXP Employee

Hello @takagi_y,

Due to the behavior of the protocol the transmitter is always listening to the bus, but you can disable the self-reception in the bit "SRX_DIS" of register "Module Configuration Register (FLEXCANx_MCR)" in the RM, where inside describes the bit functionality.

BR
Habib

0 Kudos
Reply