What are min./max operating voltages for I2C on iMXRT1064?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are min./max operating voltages for I2C on iMXRT1064?

806 Views
masoud_zahedi
Contributor I

Hi all,

What are min./max operating voltages for I2C on iMXRT1064, specifically connected to J11 (GPIO_AD_B1_00) and K11 (GPIO_AD_B1-01)?  

Thanks,

Masoud

Labels (1)
0 Kudos
Reply
1 Reply

753 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Masoud,

These values will depend on what are you supplying to NVCC_GPIO. Please refer below image, which corresponds to Table 21 from the datasheet.

pastedImage_35.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply