WebUSB on iMXRT device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WebUSB on iMXRT device

941 Views
tonythurood2
Contributor I

We are developing a product on the iMXRT1062. I would like to implement the WebUSB class on the EVKB board. When connecting the USB Device port to a PC it should enumerate a USB port and initiate a URL connection.

I can't find any examples for the required descriptors etc. Can anyone help with links to example code. It must be compatible with the NXP USB stack.

TIA.

 

0 Kudos
Reply
1 Reply

912 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

Unfortunately, there is no specific example in the SDK examples. However, I was able to find this reference in Zephyr OS: WebUSB sample application — Zephyr Project Documentation

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply