VIT solution and portuguese language

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VIT solution and portuguese language

511 Views
andréluis
Contributor II

Hello, i'm using the VIT solution, and i create a model in portuguese language. I copy the VIT_Model_pt.h to vit/CortexM7/Lib, and made the changes in code to call the model. But, in this line of code, i have a VIT_INVALID_MODEL:

#ifdef VIT_MODEL_PT
case PT:
VIT_Status = VIT_SetModel(VIT_Model_pt, MODEL_LOCATION);
break;
#endif

I want to know if i have a way to test my model, or if i made some wrong configuration in my code. Thanks for the help. 

Tags (1)
0 Kudos
Reply
6 Replies

448 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @andréluis,

How did you create the model that you are trying to use? If you use the default VIT_Model_pt.h model from the example codes, does it work properly? Or does it also give an error message?

0 Kudos
Reply

442 Views
andréluis
Contributor II

Hello, in the case i use the following link: https://vit.nxp.com/#/generate

So, i copy the model to my project and debug the firmware. And i received the error VIT_INVALID_MODEL. I tried with english too, and receive the same error, so i think it's can be the link or the creation of the model where is the problem. 

0 Kudos
Reply

422 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @andréluis,

What about using the default VIT_Model_pt.h model from the example codes, does it work properly, or does it also give an error message as well?

Are you basing your application on any example code?

0 Kudos
Reply

419 Views
andréluis
Contributor II

Hello, now i'm using the maestro_record example. My board is the MIMXRT1060-EVK. I updated my SDK to 2.16. In my example, i dont have a default model in VIT_Model_pt. I have another 10 languages, but not the portuguese. 

0 Kudos
Reply

359 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @andréluis,

Try navigating to <SDK installation folder>\SDK_2_16_000_EVK-MIMXRT1060.zip\middleware\vit\CortexM7\Lib and you should find the default VIT_Model_pt.h file. Please try importing that one.

0 Kudos
Reply

241 Views
andréluis
Contributor II

Hello, i tried the model in <SDK installation folder>\SDK_2_16_000_EVK-MIMXRT1060.zip\middleware\vit\CortexM7\Lib and it's not worked. I will try again but in the moment it's no working. How can i make this work? Thanks for the help. 

0 Kudos
Reply