VGLite Toolkit and User guide location

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VGLite Toolkit and User guide location

1,867 Views
daniel_varley
Contributor I

Hello, 

AN13778 refers to a VGLite Toolkit and user guide. Can someone please let me know where I can get access to these?

Thanks.

0 Kudos
Reply
3 Replies

1,830 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, I hope you are well.

The tool is now available: Download Page - Email Alert (nxp.com)

Out of curiosity, what are your specific needs/intentions for the tool? Which RT device are you using?

Best regards,
Omar

0 Kudos
Reply

1,814 Views
daniel_varley
Contributor I

Hello Omar, 

Thanks for the download link. I don't suppose there is any planned support for a windows based VGTLite toolkit?

I'm currently evaluating the iMXRT1170 and wanted to use VGLite and Elemental to help check general graphics performance. 

On a side note, do you know if there are any restrictions/considerations when trying to use VGLite on the CM4 core in the RT1170?

Best regards, 

Dan.

0 Kudos
Reply

1,593 Views
radoslawp
Contributor III

I was able to run vglite on CM4 and it worked really well. I had issue though when CM4 was running from SDRAM when framebuffer is also placed because such configuration didn't work so I had to run CM4 from TCM.

0 Kudos
Reply