Using i3c with i2c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using i3c with i2c

跳至解决方案
763 次查看
teruteru5678
Contributor I

I'm connecting the WM8904 to the I3C bus from the RT685 using the MIMXRT685-EVK and controlling it via I2C. Please tell me about the settings and processing for PUR in that case. [Question] 1) Is it possible to control the WM8904 using only I3CSDA and SCL and use P2_31 PUR as SWO? It seems possible to set it up, but is it okay to set it up like this? 2) When using P2_31 as PUR, is it correct to understand that it's okay to leave P2_31 unconnected as long as SDA is pulled up (e.g. 2.2kΩ)?

0 项奖励
回复
1 解答
708 次查看
Sam_Gao
NXP Employee
NXP Employee

@teruteru5678 

It is possible about your question if you only want to use I2C instead, also the PUR IO port can be used as SWO if both SCL and SDA are pulled up(R413, R414 is DNP as default) in that time.

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
696 次查看
teruteru5678
Contributor I

Sorry for the late reply.
Thank you for your reply.

0 项奖励
回复
709 次查看
Sam_Gao
NXP Employee
NXP Employee

@teruteru5678 

It is possible about your question if you only want to use I2C instead, also the PUR IO port can be used as SWO if both SCL and SDA are pulled up(R413, R414 is DNP as default) in that time.

 

0 项奖励
回复