Using both UVC and UAC in RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using both UVC and UAC in RT1060

1,383 Views
MartinYe
Contributor I

Hi,

I am trying to integrate both UVC and UAC functions with the MIMXRT1060-EVK, but found that there is only seperated sample code for just UVC or UAC in the SDK.

The sample code for UAC is "evkmimxrt1060_maestro_usb_mic" which only for FreeRTOS.

And the UVC sample code is just for virtual camera, which is "evkmimxrt1060_dev_video_virtual_camera_bm".

I hope NXP will provide a sample code which can support both UVC and UAC functions for the MIMXRT1060-EVK. Thanks a lot.

BTW, I found a similar topic "Using 2 ISO endpoint tranfer in RT1060" in the forums, but it had NOT provided a final solution yet.

0 Kudos
Reply
1 Reply

1,370 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @MartinYe ,

I'm sorry there isn't such demo. You can refer to usb_device_composite_hid_audio_unified and add UVC to it.

 

Regards,

Jing

0 Kudos
Reply