Unit of INIT_DELAY in ETC_TRIGG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unit of INIT_DELAY in ETC_TRIGG

550 Views
kurt_staubli
Contributor III

In "i.MX RT1060 Processor Reference Manual, Rev. 3, 07/2021" page 3470 INIT_DELAY is defined with the following formula:

Initial_delay = (INIT_DELAY+1)*(PRE_DIVIDER+1)*ipg_clk

What is the unit of Initial_delay? ipg_clk?

0 Kudos
Reply
1 Reply

537 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @kurt_staubli ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What is the unit of Initial_delay? ipg_clk?
-- It's the clock period of the ipg_clk
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply