Unable to get SDK_1060 with OTA_Bootloader example.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to get SDK_1060 with OTA_Bootloader example.

908 Views
tonythurood2
Contributor I

Hi, I am trying to use the SDK builder to download the OTA_bootloader example.

I select Required Example Projects

  •  

     

    ota_bootloader (bootloader_examples)

Build for MIMXRT1060-EVKB and download the zip.

The ota_bootloader does not appear in the... \SDK_2_11_1_MIMXRT1060-EVKB_ota_bootloader\boards\evkbmimxrt1060\bootloader_examples\

Only a "flashloader" example.

I have tried 3 times with no success.

Please supply an ota_bootloader_example zip or tell me how to get this code.

thanks,

Tony

 

Labels (1)
0 Kudos
Reply
3 Replies

901 Views
tonythurood2
Contributor I

That was a waste of time.

The code files in ...\SDK_2_10_0_MIMXRT1060-EVKB\boards\evkbmimxrt1060\bootloader_examples\ota_bootloader

are the same as the files in...

SDK_2_10_0_MIMXRT1060-EVKB\boards\evkbmimxrt1060\bootloader_examples\flashloader

nothing more, nothing less.

Nothing "bootloader" specific?

Have you downloaded this SDK?

 

0 Kudos
Reply

889 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
From the perspective of function, the ota_bootloader and flashloader are almost the same, however, the flashloader is only able to be executed in the RAM, in another word, the flashloader is the RAM version of the ota_bootloader.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 Kudos
Reply

903 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
For SDK_2_11, there's the mcu boot demo to replace the OTA_bootloader, and in the SDK_2_10, there's the OTA_bootloader demo.

Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply