USB on MIMXRT1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB on MIMXRT1176

Jump to solution
1,004 Views
ahmedhrabi
Contributor IV

Hi, 

I'am working on USB on the MIMXRT1176 and i have some questions: 

1- I tested CDC class VCOM, but the speed seems to be slow for my usage (~300 KB/s), am i looping something to speed up the transfer? I tested the MSC class and the transfer speed reached about 5MB/s, i don't understand why i can't reach such speed on CDC class.

2- For the CDC VNIC SDK example project, there's no lwip stack, how can i test transfer (file or data) with this example for the RNDIS class ?

3- Is there a specific recommended class to reach high speed transfer on USB ?

Regards. 

0 Kudos
Reply
1 Solution
949 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ahmedhrabi,

MSC is expected to be faster by definition. CDC often contains much more back and forth and setup data than MSC.

The lwip stack can be found on our lwip examples on the SDK.

 

BR,

Edwin.

View solution in original post

1 Reply
950 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ahmedhrabi,

MSC is expected to be faster by definition. CDC often contains much more back and forth and setup data than MSC.

The lwip stack can be found on our lwip examples on the SDK.

 

BR,

Edwin.