USB msc host fatfs freertos failures tested with EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB msc host fatfs freertos failures tested with EVK

跳至解决方案
2,761 次查看
anasnadukkandiyil
Contributor III

We are testing USB export   code on NXP EVK.

 

These is mainly 2 tasks HostTaskFn task and USB_HostApplicationTask.

Test code fails after at least  20 iteration ,during failures 

  • USB_HostTaskFn() task is waiting for OSA_EventWait()
  • Due to above scenario , USB_HostApplicationTask() will be mostly is semophore wait, since sem give is happening in USB_HostTaskFn
  • Tested by changing interrupt priority both increased & decreased but behaviour is not stable
  • Couldn't exactly identify USB_HostTaskFn() is missing interrupt  signal from ISR or ISR not generated,what cases interrupt miss

 

0 项奖励
回复
1 解答
2,639 次查看
anasnadukkandiyil
Contributor III

Issue resolved in SDK 2.13 .But integration to GUI code did not work, Rasing a separate question for that.

Re: USB host fats integration to UI did not work. - NXP Community

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,635 次查看
anasnadukkandiyil
Contributor III

Issue resolved with SDK 2.13 

New integration issue with UI raised in community  

USB host fats integration to UI did not work. - NXP Community

0 项奖励
回复
2,640 次查看
anasnadukkandiyil
Contributor III

Issue resolved in SDK 2.13 .But integration to GUI code did not work, Rasing a separate question for that.

Re: USB host fats integration to UI did not work. - NXP Community

0 项奖励
回复
2,701 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @anasnadukkandiyil,

Could you please specify what part number, SDK and IDE versions you are using?

0 项奖励
回复
2,696 次查看
anasnadukkandiyil
Contributor III

MCUXpressoIDE_11.7.0_9198

SDK_2_12_1_MIMXRT1170-EVK

0 项奖励
回复
2,717 次查看
anasnadukkandiyil
Contributor III

Is it possible to decrease the host configuration to work at USB fast speed instead of high speed irrespective of USB mass storage device capable of high speed?

0 项奖励
回复
2,670 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @anasnadukkandiyil,

I believe the following community post will be very useful for your inquiry: https://community.nxp.com/t5/i-MX-RT/How-to-change-USB-speed-HIGH-to-FULL-on-RT1064-EVB/m-p/1177751

One more thing, are the baremetal USB example codes we provide working correctly for you? If not, it might be a hardware issue rather than a software one.

0 项奖励
回复
2,655 次查看
anasnadukkandiyil
Contributor III

Thank you Bare metal version works fine, issue observed  in freertos version if I increase the  write buffer to 64KB  and do open write sync close in a loop.

 

 

/*
* Copyright (c) 2015, Freescale Semiconductor, Inc.
* Copyright 2016, 2018 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/

#include <stdio.h>
#include "usb_host_config.h"
#include "usb_host.h"
#include "usb_host_msd.h"
#include "host_msd_fatfs.h"
#include "ff.h"
#include "diskio.h"
#include "fsl_device_registers.h"
#include "app.h"
#include "samplePdf.h"
/*******************************************************************************
* Definitions
******************************************************************************/

#if MSD_FATFS_THROUGHPUT_TEST_ENABLE
#include "fsl_device_registers.h"
#define THROUGHPUT_BUFFER_SIZE (64 * 1024) /* throughput test buffer */
#define MCU_CORE_CLOCK (120000000) /* mcu core clock, user need to configure it. */
#endif /* MSD_FATFS_THROUGHPUT_TEST_ENABLE */

/*******************************************************************************
* Prototypes
******************************************************************************/

/*!
* @brief host msd control transfer callback.
*
* This function is used as callback function for control transfer .
*
* @Param param the host msd fatfs instance pointer.
* @Param data data buffer pointer.
* @Param dataLength data length.
* @status transfer result status.
*/
void USB_HostMsdControlCallback(void *param, uint8_t *data, uint32_t dataLength, usb_status_t status);

/*!
* @brief msd fatfs test code execute done.
*/
static void USB_HostMsdFatfsTestDone(void);

#if ((defined MSD_FATFS_THROUGHPUT_TEST_ENABLE) && (MSD_FATFS_THROUGHPUT_TEST_ENABLE))
/*!
* @brief host msd fatfs throughput test.
*
* @Param msdFatfsInstance the host fatfs instance pointer.
*/
static void USB_HostMsdFatfsThroughputTest(usb_host_msd_fatfs_instance_t *msdFatfsInstance);

#else

/*!
* @brief display file information.
*/
static void USB_HostMsdFatfsDisplayFileInfo(FILINFO *fileInfo);

/*!
* @brief list files and sub-directory in one directory, the function don't check all sub-directories recursively.
*/
static FRESULT USB_HostMsdFatfsListDirectory(const TCHAR *path);

/*!
* @brief forward function pointer for fatfs f_forward function.
*
* @Param data_ptr forward data pointer.
* @Param dataLength data length.
*/
#if _USE_FORWARD && _FS_TINY
static uint32_t USB_HostMsdFatfsForward(const uint8_t *data_ptr, uint32_t dataLength);
#endif

/*!
* @brief host msd fatfs test.
*
* This function implements msd fatfs test.
*
* @Param msdFatfsInstance the host fatfs instance pointer.
*/
static void USB_HostMsdFatfsTest(usb_host_msd_fatfs_instance_t *msdFatfsInstance);

#endif /* MSD_FATFS_THROUGHPUT_TEST_ENABLE */

/*******************************************************************************
* Variables
******************************************************************************/

/*! @brief msd class handle array for fatfs */
extern usb_host_class_handle g_UsbFatfsClassHandle;

usb_host_msd_fatfs_instance_t g_MsdFatfsInstance; /* global msd fatfs instance */
static FATFS fatfs;
/* control transfer on-going state. It should set to 1 when start control transfer, it is set to 0 in the callback */
volatile uint8_t controlIng;
/* control transfer callback status */
volatile usb_status_t controlStatus;

#if MSD_FATFS_THROUGHPUT_TEST_ENABLE
USB_DMA_NONINIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE)
static uint32_t testThroughputBuffer[THROUGHPUT_BUFFER_SIZE / 4]; /* the buffer for throughput test */
uint32_t testSizeArray[] = {20 * 1024, 20 * 1024}; /* test time and test size (uint: K)*/
#else
USB_DMA_NONINIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE)
static uint8_t testBuffer[(FF_MAX_SS > 256) ? FF_MAX_SS : 256]; /* normal test buffer */
#endif /* MSD_FATFS_THROUGHPUT_TEST_ENABLE */

/*******************************************************************************
* Code
******************************************************************************/

void USB_HostMsdControlCallback(void *param, uint8_t *data, uint32_t dataLength, usb_status_t status)
{
usb_host_msd_fatfs_instance_t *msdFatfsInstance = (usb_host_msd_fatfs_instance_t *)param;

if (msdFatfsInstance->runWaitState == kUSB_HostMsdRunWaitSetInterface) /* set interface finish */
{
msdFatfsInstance->runWaitState = kUSB_HostMsdRunIdle;
msdFatfsInstance->runState = kUSB_HostMsdRunMassStorageTest;
}
controlIng = 0;
controlStatus = status;
}

static void USB_HostMsdFatfsTestDone(void)
{
usb_echo("............................test done......................\r\n");
}

#if ((defined MSD_FATFS_THROUGHPUT_TEST_ENABLE) && (MSD_FATFS_THROUGHPUT_TEST_ENABLE))

static void USB_HostMsdFatfsThroughputTest(usb_host_msd_fatfs_instance_t *msdFatfsInstance)
{
uint64_t totalTime;
FRESULT fatfsCode;
FIL file;
uint32_t resultSize;
uint32_t testSize;
uint8_t testIndex;
char test_file_name[30];

/* time delay (~100ms) */
for (resultSize = 0; resultSize < 400000; ++resultSize)
{
__NOP();
}

usb_echo("............................fatfs test.....................\r\n");
CoreDebug->DEMCR |= (1 << CoreDebug_DEMCR_TRCENA_Pos);

for (testSize = 0; testSize < (THROUGHPUT_BUFFER_SIZE / 4); ++testSize)
{
testThroughputBuffer[testSize] = testSize;
}

sprintf(test_file_name, "%c:", USBDISK + '0');
fatfsCode = f_mount(&fatfs, test_file_name, 1);
if (fatfsCode)
{
usb_echo("fatfs mount error\r\n");
USB_HostMsdFatfsTestDone();
return;
}

sprintf(test_file_name, "%c:/thput.dat", USBDISK + '0');
usb_echo("throughput test:\r\n");
for (testIndex = 0; testIndex < (sizeof(testSizeArray) / 4); ++testIndex)
{
fatfsCode = f_unlink(test_file_name); /* delete the file if it is existed */
if ((fatfsCode != FR_OK) && (fatfsCode != FR_NO_FILE))
{
USB_HostMsdFatfsTestDone();
return;
}

fatfsCode = f_open(&file, test_file_name, FA_WRITE | FA_READ | FA_CREATE_ALWAYS); /* create one new file */
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}

totalTime = 0;
testSize = testSizeArray[testIndex] * 1024;
while (testSize)
{
if (msdFatfsInstance->deviceState != kStatus_DEV_Attached)
{
USB_HostMsdFatfsTestDone();
return;
}
DWT->CYCCNT = 0;
DWT->CTRL |= (1 << DWT_CTRL_CYCCNTENA_Pos);
fatfsCode = f_write(&file, testThroughputBuffer, THROUGHPUT_BUFFER_SIZE, &resultSize);
if (fatfsCode)
{
usb_echo("write error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
totalTime += DWT->CYCCNT;
DWT->CTRL &= ~(1 << DWT_CTRL_CYCCNTENA_Pos);
testSize -= THROUGHPUT_BUFFER_SIZE;
}
testSize = testSizeArray[testIndex];
usb_echo(" write %dKB data the speed is %d KB/s\r\n", testSize,
(uint32_t)((uint64_t)testSize * (uint64_t)MCU_CORE_CLOCK / (uint64_t)totalTime));

fatfsCode = f_lseek(&file, 0);
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
totalTime = 0;
testSize = testSizeArray[testIndex] * 1024;
while (testSize)
{
if (msdFatfsInstance->deviceState != kStatus_DEV_Attached)
{
USB_HostMsdFatfsTestDone();
return;
}
DWT->CYCCNT = 0;
DWT->CTRL |= (1 << DWT_CTRL_CYCCNTENA_Pos);
fatfsCode = f_read(&file, testThroughputBuffer, THROUGHPUT_BUFFER_SIZE, &resultSize);
if (fatfsCode)
{
usb_echo("read error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
totalTime += DWT->CYCCNT;
DWT->CTRL &= ~(1 << DWT_CTRL_CYCCNTENA_Pos);
testSize -= THROUGHPUT_BUFFER_SIZE;
}
testSize = testSizeArray[testIndex];
usb_echo(" read %dKB data the speed is %d KB/s\r\n", testSize,
(uint32_t)((uint64_t)testSize * (uint64_t)MCU_CORE_CLOCK / (uint64_t)totalTime));

fatfsCode = f_close(&file);
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
}

USB_HostMsdFatfsTestDone();
}

#else

static void USB_HostMsdFatfsDisplayFileInfo(FILINFO *fileInfo)
{
char *fileName;
fileName = fileInfo->fname;
/* note: if this file/directory don't have one attribute, '_' replace the attribute letter ('R' - readonly, 'H' -
* hide, 'S' - system) */
usb_echo(" %s - %c%c%c - %s - %dBytes - %d-%d-%d %d:%d:%d\r\n", (fileInfo->fattrib & AM_DIR) ? "dir" : "fil",
(fileInfo->fattrib & AM_RDO) ? 'R' : '_', (fileInfo->fattrib & AM_HID) ? 'H' : '_',
(fileInfo->fattrib & AM_SYS) ? 'S' : '_', fileName, (fileInfo->fsize),
(uint32_t)((fileInfo->fdate >> 9) + 1980) /* year */,
(uint32_t)((fileInfo->fdate >> 5) & 0x000Fu) /* month */, (uint32_t)(fileInfo->fdate & 0x001Fu) /* day */,
(uint32_t)((fileInfo->ftime >> 11) & 0x0000001Fu) /* hour */,
(uint32_t)((fileInfo->ftime >> 5) & 0x0000003Fu) /* minute */,
(uint32_t)(fileInfo->ftime & 0x0000001Fu) /* second */
);
}

static FRESULT USB_HostMsdFatfsListDirectory(const TCHAR *path)
{
FRESULT fatfsCode = FR_OK;
FILINFO fileInfo;
DIR dir;
uint8_t outputLabel = 0;

fatfsCode = f_opendir(&dir, path);
if (fatfsCode)
{
return fatfsCode;
}
while (1)
{
fatfsCode = f_readdir(&dir, &fileInfo);
if ((fatfsCode) || (!fileInfo.fname[0]))
{
break;
}
outputLabel = 1;
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);
}
if (!outputLabel)
{
usb_echo("\r\n");
}

return fatfsCode;
}

#if _USE_FORWARD && _FS_TINY
static uint32_t USB_HostMsdFatfsForward(const uint8_t *data, uint32_t dataLength)
{
uint32_t resultCount = dataLength;

if (dataLength == 0)
{
return 1;
}
else
{
do
{
usb_echo("%c", *data);
data++;
resultCount--;
} while (resultCount);
return dataLength;
}
}
#endif
char count_string[1024];
int count =0;
int written=0;
int FATret =0;
static void USB_HostMsdFatfsTest(usb_host_msd_fatfs_instance_t *msdFatfsInstance)
{
FRESULT fatfsCode;
FATFS *fs;
FIL file;
FILINFO fileInfo;
uint32_t freeClusterNumber;
uint32_t index;
uint32_t resultSize;
char *testString;
uint8_t driverNumberBuffer[3];

/* time delay */
for (freeClusterNumber = 0; freeClusterNumber < 10000; ++freeClusterNumber)
{
__NOP();
}

usb_echo("............................fatfs test.....................\r\n");

usb_echo("fatfs mount as logiacal driver %d......", USBDISK);
sprintf((char *)&driverNumberBuffer[0], "%c:", USBDISK + '0');
fatfsCode = f_mount(&fatfs, (char const *)&driverNumberBuffer[0], 0);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");

#if (FF_FS_RPATH >= 2)
fatfsCode = f_chdrive((char const *)&driverNumberBuffer[0]);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
#endif
while(1)
{
memset(count_string,'\0',sizeof(count_string));
sprintf(count_string,"%d",count);
strcat(count_string,".pdf");
FATret = f_open(&file, _T(count_string), FA_WRITE | FA_READ | FA_CREATE_ALWAYS);
if (FATret == 0 )
{
usb_echo("PDF %s Open\r\n",count_string);
FATret = f_write(&file,samplePdf_pdf,60, &written);
if (written>0)
{
usb_echo("PDF %s written %d bytes \r\n",count_string,written);
}
FATret = f_sync(&file);
if(FATret == 0 )
usb_echo("PDF %s sync successfully \r\n",count_string);
FATret = f_close(&file);
if(FATret == 0 )
usb_echo("PDF %s close successfully \r\n",count_string);
}
count++;
}
#if FF_USE_MKFS
MKFS_PARM formatOptions;
formatOptions.fmt = FM_SFD | FM_ANY;
usb_echo("test f_mkfs......");
fatfsCode = f_mkfs((char const *)&driverNumberBuffer[0], &formatOptions, testBuffer, FF_MAX_SS);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
#endif /* FF_USE_MKFS */

usb_echo("test f_getfree:\r\n");
fatfsCode = f_getfree((char const *)&driverNumberBuffer[0], (DWORD *)&freeClusterNumber, &fs);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
if (fs->fs_type == FS_FAT12)
{
usb_echo(" FAT type = FAT12\r\n");
}
else if (fs->fs_type == FS_FAT16)
{
usb_echo(" FAT type = FAT16\r\n");
}
else
{
usb_echo(" FAT type = FAT32\r\n");
}
usb_echo(" bytes per cluster = %d; number of clusters=%lu \r\n", fs->csize * 512, fs->n_fatent - 2);
usb_echo(" The free size: %dKB, the total size:%dKB\r\n", (freeClusterNumber * (fs->csize) / 2),
((fs->n_fatent - 2) * (fs->csize) / 2));

usb_echo("directory operation:\r\n");
usb_echo("list root directory:\r\n");
fatfsCode = USB_HostMsdFatfsListDirectory((char const *)&driverNumberBuffer[0]);
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("create directory \"dir_1\"......");
fatfsCode = f_mkdir(_T("1:/dir_1"));
if (fatfsCode)
{
if (fatfsCode == FR_EXIST)
{
usb_echo("directory exist\r\n");
}
else
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
}
else
{
usb_echo("success\r\n");
}
usb_echo("create directory \"dir_2\"......");
fatfsCode = f_mkdir(_T("1:/dir_2"));
if (fatfsCode)
{
if (fatfsCode == FR_EXIST)
{
usb_echo("directory exist\r\n");
}
else
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
}
else
{
usb_echo("success\r\n");
}
usb_echo("create sub directory \"dir_2/sub_1\"......");
fatfsCode = f_mkdir(_T("1:/dir_1/sub_1"));
if (fatfsCode)
{
if (fatfsCode == FR_EXIST)
{
usb_echo("directory exist\r\n");
}
else
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
}
else
{
usb_echo("success\r\n");
}
usb_echo("list root directory:\r\n");
fatfsCode = USB_HostMsdFatfsListDirectory(_T("1:"));
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("list directory \"dir_1\":\r\n");
fatfsCode = USB_HostMsdFatfsListDirectory(_T("1:/dir_1"));
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("rename directory \"dir_1/sub_1\" to \"dir_1/sub_2\"......");
fatfsCode = f_rename(_T("1:/dir_1/sub_1"), _T("1:/dir_1/sub_2"));
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("delete directory \"dir_1/sub_2\"......");
fatfsCode = f_unlink(_T("1:/dir_1/sub_2"));
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");

#if (FF_FS_RPATH >= 2)
usb_echo("get current directory......");
fatfsCode = f_getcwd((TCHAR *)&testBuffer[0], 256);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("%s\r\n", testBuffer);
usb_echo("change current directory to \"dir_1\"......");
fatfsCode = f_chdir(_T("dir_1"));
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("list current directory:\r\n");
fatfsCode = USB_HostMsdFatfsListDirectory(_T("."));
if (fatfsCode)
{
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("get current directory......");
fatfsCode = f_getcwd((TCHAR *)&testBuffer[0], 256);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("%s\r\n", testBuffer);
#endif

usb_echo("get directory \"dir_1\" information:\r\n");
fatfsCode = f_stat(_T("1:/dir_1"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);
usb_echo("change \"dir_1\" timestamp to 2015.10.1, 12:30:0......");
fileInfo.fdate = ((2015 - 1980) << 9 | 10 << 5 | 1); /* 2015.10.1 */
fileInfo.ftime = (12 << 11 | 30 << 5); /* 12:30:00 */
fatfsCode = f_utime(_T("1:/dir_1"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("get directory \"dir_1\" information:\r\n");
fatfsCode = f_stat(_T("1:/dir_1"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);

usb_echo("file operation:\r\n");
usb_echo("create file \"f_1.dat\"......");
fatfsCode = f_open(&file, _T("1:/f_1.dat"), FA_WRITE | FA_READ | FA_CREATE_ALWAYS);
if (fatfsCode)
{
if (fatfsCode == FR_EXIST)
{
usb_echo("file exist\r\n");
}
else
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
}
else
{
usb_echo("success\r\n");
}
usb_echo("test f_write......");
for (index = 0; index < 58; ++index)
{
testBuffer[index] = 'A' + index;
}
testBuffer[58] = '\r';
testBuffer[59] = '\n';
fatfsCode = f_write(&file, testBuffer, 60, (UINT *)&resultSize);
if ((fatfsCode) || (resultSize != 60))
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
fatfsCode = f_sync(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_printf......");
if (f_printf(&file, _T("%s\r\n"), "f_printf test") == EOF)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
fatfsCode = f_sync(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_puts......");
if (f_puts(_T("f_put test\r\n"), &file) == EOF)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
fatfsCode = f_sync(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_putc......");
testString = "f_putc test\r\n";
while (*testString)
{
if (f_putc(*testString, &file) == EOF)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
testString++;
}
fatfsCode = f_sync(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_seek......");
fatfsCode = f_lseek(&file, 0);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_gets......");
testString = f_gets((TCHAR *)&testBuffer[0], 10, &file);
usb_echo("%s\r\n", testString);
usb_echo("test f_read......");
fatfsCode = f_read(&file, testBuffer, 10, (UINT *)&resultSize);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
testBuffer[resultSize] = 0;
usb_echo("%s\r\n", testBuffer);
#if _USE_FORWARD && _FS_TINY
usb_echo("test f_forward......");
fatfsCode = f_forward(&file, USB_HostMsdFatfsForward, 10, &resultSize);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("\r\n");
#endif
usb_echo("test f_truncate......");
fatfsCode = f_truncate(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
f_close(&file);
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("test f_close......");
fatfsCode = f_close(&file);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("get file \"f_1.dat\" information:\r\n");
fatfsCode = f_stat(_T("1:/f_1.dat"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);
usb_echo("change \"f_1.dat\" timestamp to 2015.10.1, 12:30:0......");
fileInfo.fdate = ((uint32_t)(2015 - 1980) << 9 | 10 << 5 | 1); /* 2015.10.1 */
fileInfo.ftime = (12 << 11 | 30 << 5); /* 12:30:00 */
fatfsCode = f_utime(_T("1:/f_1.dat"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("change \"f_1.dat\" to readonly......");
fatfsCode = f_chmod(_T("1:/f_1.dat"), AM_RDO, AM_RDO);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("get file \"f_1.dat\" information:\r\n");
fatfsCode = f_stat(_T("1:/f_1.dat"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);
usb_echo("remove \"f_1.dat\" readonly attribute......");
fatfsCode = f_chmod(_T("1:/f_1.dat"), 0, AM_RDO);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");
usb_echo("get file \"f_1.dat\" information:\r\n");
fatfsCode = f_stat(_T("1:/f_1.dat"), &fileInfo);
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
USB_HostMsdFatfsDisplayFileInfo(&fileInfo);
usb_echo("rename \"f_1.dat\" to \"f_2.dat\"......");
fatfsCode = f_rename(_T("1:/f_1.dat"), _T("1:/f_2.dat"));
if (fatfsCode)
{
if (fatfsCode == FR_EXIST)
{
usb_echo("file exist\r\n");
}
else
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
}
else
{
usb_echo("success\r\n");
}
usb_echo("delete \"f_2.dat\"......");
fatfsCode = f_unlink(_T("1:/f_2.dat"));
if (fatfsCode)
{
usb_echo("error\r\n");
USB_HostMsdFatfsTestDone();
return;
}
usb_echo("success\r\n");

USB_HostMsdFatfsTestDone();
}

#endif /* MSD_FATFS_THROUGHPUT_TEST_ENABLE */

void USB_HostMsdTask(void *arg)
{
usb_status_t status;
usb_host_msd_fatfs_instance_t *msdFatfsInstance = (usb_host_msd_fatfs_instance_t *)arg;

if (msdFatfsInstance->deviceState != msdFatfsInstance->prevDeviceState)
{
msdFatfsInstance->prevDeviceState = msdFatfsInstance->deviceState;
switch (msdFatfsInstance->deviceState)
{
case kStatus_DEV_Idle:
break;

case kStatus_DEV_Attached: /* deivce is attached and numeration is done */
status = USB_HostMsdInit(msdFatfsInstance->deviceHandle,
&msdFatfsInstance->classHandle); /* msd class initialization */
g_UsbFatfsClassHandle = msdFatfsInstance->classHandle;
if (status != kStatus_USB_Success)
{
usb_echo("usb host msd init fail\r\n");
return;
}
msdFatfsInstance->runState = kUSB_HostMsdRunSetInterface;
break;

case kStatus_DEV_Detached: /* device is detached */
msdFatfsInstance->deviceState = kStatus_DEV_Idle;
msdFatfsInstance->runState = kUSB_HostMsdRunIdle;
USB_HostMsdDeinit(msdFatfsInstance->deviceHandle,
msdFatfsInstance->classHandle); /* msd class de-initialization */
msdFatfsInstance->classHandle = NULL;

usb_echo("mass storage device detached\r\n");
break;

default:
break;
}
}

/* run state */
switch (msdFatfsInstance->runState)
{
case kUSB_HostMsdRunIdle:
break;

case kUSB_HostMsdRunSetInterface: /* set msd interface */
msdFatfsInstance->runState = kUSB_HostMsdRunIdle;
msdFatfsInstance->runWaitState = kUSB_HostMsdRunWaitSetInterface;
status = USB_HostMsdSetInterface(msdFatfsInstance->classHandle, msdFatfsInstance->interfaceHandle, 0,
USB_HostMsdControlCallback, msdFatfsInstance);
if (status != kStatus_USB_Success)
{
usb_echo("set interface fail\r\n");
}
break;

case kUSB_HostMsdRunMassStorageTest: /* set interface succeed */
#if ((defined MSD_FATFS_THROUGHPUT_TEST_ENABLE) && (MSD_FATFS_THROUGHPUT_TEST_ENABLE))
USB_HostMsdFatfsThroughputTest(msdFatfsInstance); /* test throughput */
#else
USB_HostMsdFatfsTest(msdFatfsInstance); /* test msd device */
#endif /* MSD_FATFS_THROUGHPUT_TEST_ENABLE */
msdFatfsInstance->runState = kUSB_HostMsdRunIdle;
break;

default:
break;
}
}

usb_status_t USB_HostMsdEvent(usb_device_handle deviceHandle,
usb_host_configuration_handle configurationHandle,
uint32_t eventCode)
{
usb_status_t status = kStatus_USB_Success;
usb_host_configuration_t *configuration;
uint8_t interfaceIndex;
usb_host_interface_t *interface;
uint32_t infoValue = 0U;
uint8_t id;

switch (eventCode)
{
case kUSB_HostEventAttach:
/* judge whether is configurationHandle supported */
configuration = (usb_host_configuration_t *)configurationHandle;
for (interfaceIndex = 0; interfaceIndex < configuration->interfaceCount; ++interfaceIndex)
{
interface = &configuration->interfaceList[interfaceIndex];
id = interface->interfaceDesc->bInterfaceClass;
if (id != USB_HOST_MSD_CLASS_CODE)
{
continue;
}
id = interface->interfaceDesc->bInterfaceSubClass;
if ((id != USB_HOST_MSD_SUBCLASS_CODE_UFI) && (id != USB_HOST_MSD_SUBCLASS_CODE_SCSI))
{
continue;
}
id = interface->interfaceDesc->bInterfaceProtocol;
if (id != USB_HOST_MSD_PROTOCOL_BULK)
{
continue;
}
else
{
if (g_MsdFatfsInstance.deviceState == kStatus_DEV_Idle)
{
/* the interface is supported by the application */
g_MsdFatfsInstance.deviceHandle = deviceHandle;
g_MsdFatfsInstance.interfaceHandle = interface;
g_MsdFatfsInstance.configHandle = configurationHandle;
return kStatus_USB_Success;
}
else
{
continue;
}
}
}
status = kStatus_USB_NotSupported;
break;

case kUSB_HostEventNotSupported:
break;

case kUSB_HostEventEnumerationDone:
if (g_MsdFatfsInstance.configHandle == configurationHandle)
{
if ((g_MsdFatfsInstance.deviceHandle != NULL) && (g_MsdFatfsInstance.interfaceHandle != NULL))
{
/* the device enumeration is done */
if (g_MsdFatfsInstance.deviceState == kStatus_DEV_Idle)
{
g_MsdFatfsInstance.deviceState = kStatus_DEV_Attached;

USB_HostHelperGetPeripheralInformation(deviceHandle, kUSB_HostGetDevicePID, &infoValue);
usb_echo("mass storage device attached:pid=0x%x", infoValue);
USB_HostHelperGetPeripheralInformation(deviceHandle, kUSB_HostGetDeviceVID, &infoValue);
usb_echo("vid=0x%x ", infoValue);
USB_HostHelperGetPeripheralInformation(deviceHandle, kUSB_HostGetDeviceAddress, &infoValue);
usb_echo("address=%d\r\n", infoValue);
}
else
{
usb_echo("not idle msd instance\r\n");
status = kStatus_USB_Error;
}
}
}
break;

case kUSB_HostEventDetach:
if (g_MsdFatfsInstance.configHandle == configurationHandle)
{
/* the device is detached */
g_UsbFatfsClassHandle = NULL;
g_MsdFatfsInstance.configHandle = NULL;
if (g_MsdFatfsInstance.deviceState != kStatus_DEV_Idle)
{
g_MsdFatfsInstance.deviceState = kStatus_DEV_Detached;
}
}
break;

default:
break;
}
return status;
}

0 项奖励
回复