USB grounding when not used

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB grounding when not used

1,080件の閲覧回数
JRIIS
NXP Employee
NXP Employee

NCR from UK would like to take the opportunity to ask a question related to the VDD_USB_CAP pin.

In the our documentation (IMXRT1060RM Rev. 3, 07/2021) shows that a capacitor connected to GND is needed for this pin (please see the image shown below).

 

JRIIS_0-1647512217572.png

 

NCR not planning to use the USB, so my question is: Can they leave VDD_USB_CAP pin floating?

Thanks,

/Jakob

0 件の賞賛
返信
3 返答(返信)

1,074件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @JRIIS ,

Please refer to RT1060 datasheet.

Unused pins: USB_OTG1_CHD_B, USB_OTG1_DN, USB_OTG1_DP, USB_OTG1_VBUS, USB_OTG2_DN, USB_OTG2_DP, USB_OTG2_VBUS, leave it as floating, not connected.
https://www.nxp.com.cn/docs/en/nxp/data-sheets/IMXRT1060CEC.pdf

 

Regards,

Jing

0 件の賞賛
返信

1,064件の閲覧回数
JRIIS
NXP Employee
NXP Employee

Hi Jing - Thanks for the information. Unfortunately, what you quoted on your email below does not make any reference to the VDD_USB_CAP pin. So I am afraid that the question if the VDD_USB_CAP pin can be left unconnected still remains.

Could I kindly ask to look at this again please?

Thanks,

/Jakob

0 件の賞賛
返信

1,049件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @JRIIS ,

You can keep USB pins floating. If  USB VBUS is not applied, there is no need to connect the VDD_USB_CAP.

 

Regards,

Jing

0 件の賞賛
返信