USB Audio device class (i.MXRT1050) doesn't work on Windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Audio device class (i.MXRT1050) doesn't work on Windows 10

2,523件の閲覧回数
dav1
Contributor V

Hi,

The USB Audio device class example (usb speaker) for the i.MXRT1050 doesn't work on Windows 10.

it plays for 0.5sec then stops. Any chance we can see an update soon? Preferably incl. UAC2.0.

ps. works great on macOS.

Team NXP,

  • can we get in touch with the people that wrote this Audio Device class driver?
  • is there a list of OS'es this has been tested against? (linux, mac, iOS, windows, android)!?
  • is there a git-repository for the driver-code so where the development/patches so far can be followed!?
ラベル(1)
5 返答(返信)

2,031件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Have you tried the example avoiding using USB HUBs and direct connection to computer’s USB ports instead?

Regarding driver availability, they are released on each SDK version release, and their changes are summarized on the Release Notes document of each release.

In case of requiring a custom implementation of the USB Audio driver, you could consider NXP Professional Services.

For more information regarding this, please refer to the following link:

https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,031件の閲覧回数
dav1
Contributor V

Hi, Any updates to this in the latest SDK_2.6.1?

not sure where to find the release-notes / history for a specific driver.

0 件の賞賛
返信

2,031件の閲覧回数
dav1
Contributor V

Hi Carlos,

1. Sounds like this could be in the USB core itself then, probably not handling "non multi-tt hubs correctly" or USB split transactions. Can you please file a bug-report to get this resolved?

2. What is the purpose of these drivers, demo or production use? Is there a list available on how these have been tested, what os'es etc!?

Thanks David

0 件の賞賛
返信

2,031件の閲覧回数
dav1
Contributor V

ping. any plans to continue work, making the audio host/device driver for RT-series more stable?

0 件の賞賛
返信

2,031件の閲覧回数
dav1
Contributor V

ping again

0 件の賞賛
返信