UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

跳至解决方案
1,988 次查看
takayuki_ishii
Contributor V

Hello community,

 

I have 2 question about eFUSE bit of IMXRT1170.

In RT1170 Reference Manual Table 26-7. Boot parameter fusemap,

BOOT_PARAM4 have 2 SDP_DISABLE bit.

Which function does it select enable/disable?

1) UART_SDP_DISABLE : BOOT_PARAM4[1]

2) SDP_DISABLE : BOOT_PARAM4[0]

 

Best regards,

Ishii.

 

标记 (1)
0 项奖励
回复
1 解答
1,981 次查看
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,982 次查看
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

0 项奖励
回复
1,975 次查看
takayuki_ishii
Contributor V

Hello jay_heng,

 

Thank you for your quick reply.

I will answer it to my customer.

 

Best regards,

Ishii.

 

0 项奖励
回复