UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

ソリューションへジャンプ
2,003件の閲覧回数
takayuki_ishii
Contributor V

Hello community,

 

I have 2 question about eFUSE bit of IMXRT1170.

In RT1170 Reference Manual Table 26-7. Boot parameter fusemap,

BOOT_PARAM4 have 2 SDP_DISABLE bit.

Which function does it select enable/disable?

1) UART_SDP_DISABLE : BOOT_PARAM4[1]

2) SDP_DISABLE : BOOT_PARAM4[0]

 

Best regards,

Ishii.

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,996件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,997件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

0 件の賞賛
返信
1,990件の閲覧回数
takayuki_ishii
Contributor V

Hello jay_heng,

 

Thank you for your quick reply.

I will answer it to my customer.

 

Best regards,

Ishii.

 

0 件の賞賛
返信