Hello community,
I have 2 question about eFUSE bit of IMXRT1170.
In RT1170 Reference Manual Table 26-7. Boot parameter fusemap,
BOOT_PARAM4 have 2 SDP_DISABLE bit.
Which function does it select enable/disable?
1) UART_SDP_DISABLE : BOOT_PARAM4[1]
2) SDP_DISABLE : BOOT_PARAM4[0]
Best regards,
Ishii.
Solved! Go to Solution.
Both UART and USB port can be used as SDP interface in BootROM.
SDP_DISABLE bit - whole SDP interfaces
UART_SDP_DISABLE bit - just UART port
Both UART and USB port can be used as SDP interface in BootROM.
SDP_DISABLE bit - whole SDP interfaces
UART_SDP_DISABLE bit - just UART port
Hello jay_heng,
Thank you for your quick reply.
I will answer it to my customer.
Best regards,
Ishii.