Tracealyzer not working with iMXRT1060 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tracealyzer not working with iMXRT1060 EVK

872 Views
EmbeddedTech
Contributor III

Hi,

 I have iMXRT1060EVK and would like to use the Tracealyzer in streaming mode for FreeRTOS. I am using IAR EW and I-jet debugging probe. I have followed the procedure as in the links below but still have issues with data streaming. I cannot see any data on the trace.

Is there anything specific to be done on iMXRT1060 EVK boards for tracealyzer to work?

Is there any document that describes the steps required to enable trace data?

https://percepio.com/wp-content/uploads/2022/07/PA023-Streaming-over-Arm-ITM-IAR.pdf

https://www.youtube.com/watch?v=1MO2kDTJnyg

https://percepio.com/tracealyzer/gettingstarted/iar/

Your help on this is highly appreciated.

 

Thanks

0 Kudos
Reply
2 Replies

853 Views
JohanKraft
Contributor I

Can you transmit data using ITM and see it in the IAR Terminal I/O window? For example, ITM_SendChar('X');

Otherwise you may need to enable SWO output on the device. See https://www.nxp.com/docs/en/application-note/AN13234.pdf

0 Kudos
Reply

844 Views
EmbeddedTech
Contributor III

Hi,

I was able to see the ITM data on the IAR terminal only after doing the modification required for the SWO. There is no mention anywhere about the procedure to be followed for Tracealyzer for iMXRT. After some googling, I found that application note and tried it. But still, I have issues with getting Tracealyzer traces. I am liasing with the support team for now.

Thanks.

0 Kudos
Reply