Hi All,
I have been trying to understand the various trace options with the iMXRT1021, IAR Embedded Workbench, and J-Link connected via SWD (just SWDIO and SWCLK pins).
(As an aside, with the 100pin iMXRT1021, you cannot use SWO or TRACE[] if you want to use Ethernet in your application - this seems like a very poor choice of pin allocation for a communications processor!!)
I believe I can use ETM configured to fill the ETB, and get the information out through the J-Link.
Am I right? Is there any code I need to run in my project to configure the ETM / ETB? Or should it be done by the IAR tools?
Thanks,
Chris.