The test data for P2020 Ethernet forwarding performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The test data for P2020 Ethernet forwarding performance

1,090 Views
wqking1000
Contributor I

1.Where are you about performance test data for p2020 Ethernet forwarding? And corresponding methods and test tools?

2.Where are you about performance test data for p2020 Ethernet Nat Firewall forwarding? And corresponding methods and test tools?

3.Where are you about performance test data for p2020 Ethernet ipsec ? And corresponding methods and test tools?

Tags (2)
0 Kudos
Reply
1 Reply

1,061 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 琦 王,

Please refer to the following test data, the test tool is Spirent TestCenter.

1. IPv4 fwd 2 cores 2G

FrameSize(Bytes)  Throughputs(Mbps)

64               400

128              700.63

256              1286.5

390              1901.39

512              2000.0

1024             2000.0

1280             2000.0

1518             2000.0

2.Ipv4 Nat firewall 2 core 1 flow

FrameSize(Bytes)       Throughput(Mbps)

66                                95.08

128                             163.72

256                             304.87

512                             584.28

1024                          999.03

1280                          999.03

1518                          999.03

3. IPv4 SEC 3DES_SHA1 2core 2G

FrameSize(Bytes)    Througput(Mbps)

82                 112.81

408                385.45

1442               1282.64

IPv4 SEC AES_SHA1 2core 2G

FrameSize(Bytes)    Througput(Mbps)

82                 112.81

408                387.38

1442               1286.5

Thanks,

Yiping

0 Kudos
Reply