Source for sdphost and blhost?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Source for sdphost and blhost?

8,108 次查看
rshipman
Senior Contributor I

Hi,

Is it possible to get the source to sdphost and blhost please?

Thanks and regards,

Ronnie

标签 (1)
0 项奖励
回复
3 回复数

8,009 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ronnie, 

To get the source code of these two tools, you need to download the SDK for any RT and include the optional mcu-boot under middleware when building your SDK package in the SDK builder. This option adds in flashloader and tools source files. They'll be found in the middleware/mcu-boot/tools/tools folder.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

7,973 次查看
ruudmeer
Contributor II

I think I did what proposed. I selected mcu-boot and dowloaded the SDK.
I did get the tools directory but only found sources for sdphost.

So not for blhost  !!

What should I do to get these sources?

 

0 项奖励
回复

7,442 次查看
wolfgangreich
Contributor I
0 项奖励
回复