Source for sdphost and blhost?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Source for sdphost and blhost?

8,274件の閲覧回数
rshipman
Senior Contributor I

Hi,

Is it possible to get the source to sdphost and blhost please?

Thanks and regards,

Ronnie

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

8,175件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ronnie, 

To get the source code of these two tools, you need to download the SDK for any RT and include the optional mcu-boot under middleware when building your SDK package in the SDK builder. This option adds in flashloader and tools source files. They'll be found in the middleware/mcu-boot/tools/tools folder.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

8,139件の閲覧回数
ruudmeer
Contributor II

I think I did what proposed. I selected mcu-boot and dowloaded the SDK.
I did get the tools directory but only found sources for sdphost.

So not for blhost  !!

What should I do to get these sources?

 

0 件の賞賛
返信

7,608件の閲覧回数
wolfgangreich
Contributor I
0 件の賞賛
返信