Smartwatch GUI Demo Images for the NXP i.MX RT500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Smartwatch GUI Demo Images for the NXP i.MX RT500

Jump to solution
2,765 Views
ssnider
Contributor III

Looking to develop a smartwatch or wearable device for the i.MX RT500 crossover MCU?

To help you visualize the graphical performance of it, we’ve created two full-feature smartwatch demo applications for you to try on your NXP i.MX hardware. Within moments, you'll be able to interact with a fully functional GUI application and see the touch screen sensitivity and graphical performance that the i.MX RT500 provides.

See it in action here - watch video

Simply request a version for download for your NXP hardware.

1 Solution
2,715 Views
ssnider
Contributor III

If you would like to see the details behind this demo image being built in Storyboard (and it in action), check out this webinar we recently did with NXP.

View solution in original post

3 Replies
2,716 Views
ssnider
Contributor III

If you would like to see the details behind this demo image being built in Storyboard (and it in action), check out this webinar we recently did with NXP.

2,721 Views
ssnider
Contributor III

Not a problem at all. There are plenty of other demo images available for download for other NXP hardware here as well.

Cheers,
Scott

0 Kudos
Reply
2,729 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thank you, Ssnider!

Looks neat! Definitely a great option when creating GUIs!

Regards,
Gustavo

0 Kudos
Reply