Is there a way of provisioning an RT1021 so that it can be done by a third party without compromising the software IP?
I've come to the conclusion that the answer is no, because you need a trusted person to first burn the fuses/keys etc into the RT1021 and any secure code into flash.
I was just wondering if anyone had some thoughts on this?
Ideally we would like to outsource the manufacturing of the entire product, but I don't think we can because the RT1021 needs provisioning securely.
Hi @rshipman ,
Maybe you can connect RT with a SE like SE050E2 and use the keys inside the SE instead, you know , the keys in SE are trust provisioned out of factory by NXP.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------